Your Power Questions... Answered!
Our application manager, Alan Hill is back with more information about the best way to select a power supply when peak load is the major deciding factor.
Recommended for you

The CCP550 Series
550W open-frame power supplies with multiple cooling options

The HPF3K0 Series
The HPF is a highly flexible, single-phase solution ideal for a wide range of healthcare, semiconductor manufacturing an...

HPF3K0 - Programming interface
A brief introduction to the ease of installation and configuration of the HPF3K0 3kW programmable power supplies.

HPA Series
The HPA offers rapid user configurability from an extremely compact, high power density, low profile 1U module.