Resources
Filter by
![](https://www.xppower.com/storage/resources/images/blog/system_emi.jpg)
Determine System EMI Characteristics Early in System Design Phase
Often in the commercial, industrial, medical and military industries, system engineers wait until system qualification b...
![](https://www.xppower.com/storage/resources/images/video/ecp180_video.jpg)
ECP180 series of power supplies
120 Watts with convection-cooling and 180 Watts with force-cooling, all in a 2 x 4 x 1" package.
![](https://www.xppower.com/storage/resources/images/blog/MIL-STD-1275.jpg)
MIL-STD-1275 Compliance for power systems made easy.
The US Department of Defense Standard MIL-STD 1275 is an immunity standard that defines a series of test conditions to b...
![](https://www.xppower.com/storage/resources/images/blog/batteries.jpg)
Supplying an AC-DC Power Supply from a DC source
A frequently asked question concerns the suitability of using an AC/DC power supply with a DC source. There are two part...
![](https://www.xppower.com/storage/resources/images/press-releases/qsb150pr.jpg)
150 Watt Half Brick DC/DC Wandler mit außergewöhnlich weitem 8:1 Eingangsspannungsbereich
XP Power stellt heute mit der QSB150 Serie seine neuen 150W DC/DC Wandler im Half Brick Format vor.
![](https://www.xppower.com/storage/resources/images/video/shp-mhp_video.jpg)
Rugged, industrial construction, SHP-MHP series of power supplies
SHP and MHP Series AC-DC power supplies designed to meet industrial and medical approvals.
![](https://www.xppower.com/storage/resources/images/blog/Def-stan-59-411.jpg)
DEF-STD 59-411 and the challenge of Land Class A
DEF STD 59-411 was issued by the UK Ministry of Defence in 2007 for land, sea and air equipment. It replaced DEF STD 59...
![](https://www.xppower.com/storage/resources/images/blog/harmoniccurrentstandard.jpg)
New Version of EN61000-3-2, The Harmonic Current Standard
EN61000-3-2:2006+A2:2009 is the present standard for limits for harmonic current emissions for equipment with an input c...
![](https://www.xppower.com/storage/resources/images/blog/EPL225.jpg)
Industry leading 95% efficient 225 Watt AC-DC supply in a 2" x 4" package
The EPL225 series of high efficiency, open frame, AC-DC power supplies are approved for industrial, IT and medical appli...
![](https://www.xppower.com/storage/resources/images/blog/safety-IEC62368.jpg)
The New Safety Standard for ITE and AV Equipment: IEC62368-1
The boundaries between information technology and audio/ video technology have become increasingly blurred. For example,...
![](https://www.xppower.com/storage/resources/images/press-releases/itzpr.jpg)
Kleinster isolierter, geregelter 9W DC/DC Wandler mit 4:1 Eingang
XP Power stellt heute mit den ITZ seine neuen, kompakten DC/DC Wandler mit 9W vor. Unserer Meinung nach sind dies die kl...
![](https://www.xppower.com/storage/resources/images/blog/UsingYcapacitors.jpg)
Using Y rated capacitors in medical applications
The medical standard IEC60601-1 is mandatory for medical equipment and requires manufacturers to review the isolation sy...